Keyboard shortcut: [F7]
Function: The command sets a permanent predefined value to a variable on the controller.
Call: “Debug” menu
Requirement: The application is in online mode.




CAUTION

Unusual changes to variable values in an application currently running on the controller can cause undesired behavior of the controlled plant.
Evaluate possible dangers before forcing variable values, and take the respective safety precautions. Depending on the controlled plant, this could result in damage to the plant or the workpieces, or injury or death of personnel.
With the command, CODESYS permanently sets one or more variables of the active application to defined values on the controller.
A forced value is marked with the forced
symbol.
For more information about the functionality of forcing and the p of values, see the "Forcing and Writing of Variables" help page.
By default, the “Force Values [All Applications]” command, which applies to all application in the project, and is not included in a menu.
For more information, see: ⮫ “Forcing and Writing of Variables ” and ⮫ “Using Watch Lists ”