The Syslog client can be used to send logging messages to a SysLog server, where they can be centrally processed. In an AC500 V3 PLC it is connected to the audit logger. When the Syslog client is configured in a PLC application, all audit logger messages will be sent to the specified Syslog server.
The Syslog client is available for all AC500 V3 PLC types, except the PM5012-ETH.