NOTICE

We recommend configuring an HTTPS connection (encryption with SSL/TLS) between the visualization clients and the web server to protect the system from unwanted access.
-
Generate or import a certificate for the web server
Ensure the PLC clock is set to the current time and date when using certificates on the PLC. Otherwise the certificate cannot be used to secure a protocol (see also ⮫ “AC500 battery” and ⮫ “(S)NTP client configuration”).
-
Attach a web server node to either ETH1 or ETH2 or both and configure security mode.
This will automatically insert a visualization into the project.
The available modes of operation are:
-
http only
-
https only
-
Both (http and https)
-
Redirect http to https
-
-
Download and set the PLC to RUN.
-
Connect to the web server using the configured method: https://<your PLC´s IP address>/webvisu.htm.
In case you are using a self-signed certificate, your browser will show some warnings.
If you are aware of the risks of self-signed certificates, this can be ignored.