WARNING_ID (ENUM)

TYPE WARNING_ID

Enumeration of the Last Warning ID, describes the details of each Warning ID generated by library function blocks.

Attributes:
qualified_only
InOut:

Name

Initial

Comment

NO_WARNING

16#0

No warning

FUNCTION_INTERRUPTED

16#8010

Read or Write Parameter could not be completed

FUNCTION_ABORTED

16#8011

Function aborted

COM_DIFFERENT_LINE

16#8012

Com interface differs from the actually assigned COM by other blocks on same LineToken variable

NO_CONNECTION_COM_BLOCK

16#8013

No connection to communication block, or error in communication block