ERROR_ID (ENUM)
TYPE ERROR_ID
- Attributes:
qualified_only- InOut:
Name
Initial
Comment
NO_ERROR
16#0
No error
INVALID_COM_PORT
16#1
Specified COM port is invalid, check ID or existence of COM port in configuration
MISSING_PARAM_LIST_BUFFER
16#2
Missing reference to parameter list
PARAM_LIST_BUFFER_TOO_SMALL
16#3
Parameter list is not large enough or empty
CFG_READ_FAILED
16#4
Failed to obtain configuration data
UNKNOWN_ERROR
16#FE
unknown error occurred
DEVICE_NOT_FOUND
16#101
Device/protocol not found in device tree
PARAMETERS_NOT_FOUND
16#102
Failed to copy interface parameters
DEVICE_ALREADY_INACTIVE
16#103
Device/protocol is already inactive
DEVICE_ALREADY_ACTIVE
16#104
Device/protocol is already active
CONFIG_FAILED
16#107
Asyncrconous execution of configuration failed
CONFIG_TIMEOUT
16#108
Asyncrconous execution of configuration timed out
CONFIG_BUSY
16#109
Configuration of any serial interface / protocol is already pending, try again later
FATAL_ERROR
16#5FFF
fatal error state