ERROR_ID (ENUM)

TYPE ERROR_ID

ERROR_ID is an Enumeration to indicate error and faults of the function blocks AsciiRead & AsciiWrite

Attributes:
qualified_only
InOut:

Name

Initial

Comment

BUSY

16#9999

Busy state - Method is in procedure state

NO_ERROR

16#0

No error

INVALID_COM_PORT

16#1

Specified COM port is invalid, check ID or existence of COM port in configuration

MISSING_PARAM_LIST_BUFFER

16#2

Missing reference to parameter list

PARAM_LIST_BUFFER_TOO_SMALL

16#3

Parameter list is not large enough or empty

CFG_READ_FAILED

16#4

Failed to obtain configuration data

INVALID_INPUT_BUFFER

16#5

Invalid input data buffer - faulty reference

INVALID_INPUT_BUFFER_SIZE

16#6

Missing interface for serial connection - Input 3

INVALID_COM_ID

16#7

INVALID_SIZE_TELEGRAM_ENDING_CHAR

16#8

UNKNOWN_ERROR

16#FE

unknown error occurred

UNKNOWN_ERROR_OPEN

16#100

unknown error occurred during OPEN Com port - check AddErrNo

UNKNOWN_ERROR_READ

16#101

unknown error occurred during READ Com port - check AddErrNo

UNKNOWN_ERROR_WRITE

16#102

unknown error occurred during WRITE Com port - check AddErrNo

UNKNOWN_ERROR_CLOSE

16#103

unknown error occurred during CLOSE Com port - check AddErrNo

ERR_RECEIVED_MSG_TOO_LONG

16#200

ERR_CREATING_SERIAL_CON_INST

16#201

ERR_CHAR_LEN_TOO_SMALL

16#202

ERR_BUFFER_OVERFLOW

16#203

FATAL_ERROR

16#5FFF

fatal error state