Param (PARAMS)
- Attributes:
qualified_only- InOut:
Scope
Name
Type
Initial
Comment
Constant
CharLength
UDINT255
Maximum character length of the message. Can be modified before compile in the library manager
InternalBufferSize
UDINT5000
Describes the internal buffer size of the AsciiRead function block. Incoming telegrams are stored in the internal buffer before they are validated and executed. Can be modified according to the own needs in the application.