MC_CombineAxes (FB)

FUNCTION_BLOCK MC_CombineAxes

This function block combines the motion of 2 axes into a third axis with selectable combination method.

../../../../../../_images/plcopen.png

Basically it is a calculation of a new position setpoint based on the two position setpoints of the input axes. This function block is reflected in the state diagram like a synchronized motion type. As application example one can work with a separate profile synchronized to an object on a moving belt, or a rotating knife with flexible covered distance to be cut.

Note

To stop the motion, the function block has to be interrupted by another function block issuing a new command.

Example of Ice-cream

../../../../../../_images/MC_CombineAxes_Ex1.png

MC_CombineAxes can generate special synchronized movements that are not possible or complex to generate in other ways. In the following example, a CAM function block and the result of a Gear function block are both synchronized to a conveyor master, are added to generate a virtual master for a MC_GearInPos function of the final axis that will execute the movement. The particular application of this example could be a machine to deposit the icecream waving layers on top of the icecream base travelling through the freezer line in icecream factory. The dosing axis has to synchronize with a waving manner to the conveyor carrying the icecream base block. And it has to do this in a particular starting position and wave phase to achieve the expected result (therefore the GearInPos). With the CAM function block one can define different wave patterns easily (like the one longer in the top of icecream).

Another case application can be chocolate bars with decoration (individual bars in mouldings). The dosificator makes the wave synchronized with conveyor and returns for the next

Application example of MC_CombineAxes

../../../../../../_images/MC_CombineAxes_Ex2.png
The corresponding timing diagram for MC_CombineAxes example

../../../../../../_images/MC_CombineAxes_Ex3.png

Note

This block has to be called within the REAL-TIME task, same task as CMC_BASIC_KERNEL

InOut:

Scope

Name

Type

Comment

Input

Execute

BOOL

Starts the function block at rising edge

CombineMode

BOOL

FALSE = Addition of two input axes positions, TRUE = Subtraction of two input axes positions

GearRatioNumeratorM1

INT

Gear ratio numerator for master axis 1 towards the slave

GearRatioDenumeratorM1

INT

Gear ratio denominator for master axis 1 towards the slave

GearRatioNumeratorM2

INT

Gear ratio numerator for master axis 2 towards the slave

GearRatioDenumeratorM2

INT

Gear ratio denominator for master axis 2 towards the slave

MasterValueSourceM1

MC_Source

Decide to use the actual position or reference position of master axis 1. mcSetValue: Synchronization on master set value. mcActualValue: Synchronization on master actual value

MasterValueSourceM2

MC_Source

Decide to use the actual position or reference position of master axis 2. mcSetValue: Synchronization on master set value. mcActualValue: Synchronization on master actual value

Acceleration

LREAL

[u/s°°2] Value of the acceleration (increasing energy of the motor), just applied until “insync” is reached. Range: >0. If value = 0, Acceleration will be equal to parameter paraMaxAccelerationAppl.If value > 0 and <= 1,Acceleration will be limited to 1.

Deceleration

LREAL

[u/s°°2] Value of the deceleration (decreasing energy of the motor), just applied until “insync” is reached. Range: >0. If value = 0, Deceleration will be equal to parameter paraMaxDecelerationAppl.If value > 0 and <= 1,Deceleration will be limited to 1.

BufferMode

MC_BufferMode

Not supported, default mcABORTING used

Output

InSync

BOOL

Commanded gearing completed

Busy

BOOL

The function block is not finished

Active

BOOL

Indicates that the function block has control on the axis

CommandAborted

BOOL

Command is aborted by another command from other PLCopen function block

Error

BOOL

Signals that error has occurred within function block

ErrorID

ERROR_ID

Error identification. For error details refer to Enumeration ERROR_ID

Inout

Master1

Axis_Ref

Reference to master axis 1

Master2

Axis_Ref

Reference to master axis 2

Slave

Axis_Ref

Reference to slave axis