MC_StepAbsSwitch (FB)

FUNCTION_BLOCK MC_StepAbsSwitch

This function block performs a homing function by searching for an absolute positioned external physical switch. An Absolute Switch has two “Off” or “On” areas, see example.

For central Motion Control implementation: The signal of the Absolute Switch has to be written to the variable “absRefSwitch” of the data type CMC_Axis_IO

../../../../../../_images/plcopen.png

Note

Inside the operation area the limit switches have to be logically FALSE and outside the borders the signal of the corresponding limit switch has to be logically TRUE. If needed the signal from the sensor must be inverted before it is connected to an element the CMC_Axis_IO data type

Example

../../../../../../_images/MC_StepAbsSwitch_Ex1.png

This physical layout has the risk that homing is started in the wrong direction (escaping the switch). To support such case, it implements a special behavior when Limit Switches are found (or the AbsSwitch itself is “On” at Execute)-

  • Axis State is set to Homing,

  • The homing is commanded in the most likely direction were the sensor can be found. In this example(-),

  • The velocity is defined by the input,

  • Both time and distance limits can cause an error if exceeded,

  • If any LimitSwitch is found during Homing (any of them), then a special process is started in the opposite direction, the AbsSwitch is searched to switch off (or “On” depending on SwitchMode setting). The Edge (passed by), and homing process is restarted in the original direction and with the same conditions. This ensures that the end conditions are always same,

  • If the SwitchMode is either MC_SwitchNegative or MC_SwitchPositive, then the special process is also started in opposite direction depending from the switch state at “Execute”,

  • The direction changes only when the specified Velocity is reached (InVelocity),

  • This function block does not modify the actual position,

  • This function block does not leave the Homing State when done.

  • This function block can only be used once for a homing sequence

../../../../../../_images/MC_StepAbsSwitch_Ex2.png ../../../../../../_images/MC_StepAbsSwitch_Ex3.png

An overlapping switch configuration is also possible. This has same the behavior as working on the limit switches

../../../../../../_images/MC_StepAbsSwitch_Ex4.png

If the input direction is set to a fixed direction (MC_Positive or MC_Negative), then the initial switch state is ignored (used for example in rotary axis where only one sense of rotation is allowed):

../../../../../../_images/MC_StepAbsSwitch_Ex5.png

Note

With an overlapping switch configuration either MC_EdgeOn or MC_EdgeOff can be used for the input SwitchMode. This depends on the switching behaviour of the absolute switch and the used option for the input Direction

InOut:

Scope

Name

Type

Comment

Input

Execute

BOOL

Starts the function block at rising edge

Direction

MC_Homing_Direction

Specifies the direction of the motion if any:
  • MC_Positive = Starts in positive direction always

  • MC_Negative = Starts in negative direction always

  • MC_SwitchPositive = Depends on Switch status at Execute edge. If Switch is “Off”, direction is positive, if “On” it is negative

  • MC_SwitchNegative = Like previous, but opposite

SwitchMode

MC_Homing_Edge

Sensor condition to finalize this function block in any switch mode:
  • MC_On = When sensor is ON.

  • MC_Off = When sensor is OFF.

  • MC_EdgeOn = When Off to On transition in sensor

  • MC_EdgeOff = When On to Off transition in sensor

Velocity

LREAL

[u/s] Value of the maximum velocity (not necessarily reached). Range: >0

Acceleration

LREAL

[u/s°°2] Value of the acceleration (increasing energy of the motor). Range: >0.If value = 0, Acceleration will be equal to parameter paraMaxAccelerationAppl.If value > 0 and <= 1,Acceleration will be limited to 1.

Deceleration

LREAL

[u/s°°2] Value of the deceleration (decreasing energy of the motor). Range: >0.If value = 0, Deceleration will be equal to parameter paraMaxDecelerationAppl.If value > 0 and <= 1,Deceleration will be limited to 1.

TorqueLimit

LREAL

Not supported

TimeLimit

LREAL

[s] If the function block condition is not met in the TimeLimit, an error is issued. <=0: No time limit

DistanceLimit

LREAL

[u] If the function block condition is not met within a DistanceLimit travel, an error is issued. 0 = No distance limit

BufferMode

MC_BufferMode

Not supported, default mcABORTING used

Output

Done

BOOL

Shows the status of the function block. Done = TRUE if the execution is finished

Busy

BOOL

The function block is not finished

Active

BOOL

Indicates that the function block has control on the axis

CommandAborted

BOOL

Command is aborted by another command from other PLCopen function block

Error

BOOL

Signals that error has occurred within function block

ErrorID

ERROR_ID

Error identification. For error details refer to Enumeration ERROR_ID

Specific Error numbers: + MC_TimeLimitExceeded + MC_DistanceLimitExceeded + MC_TorqueLimitExceeded

Inout

Axis

Axis_Ref

Reference to axis