Sgx_CALIBRATION_INDEX (ENUM)
TYPE Sgx_CALIBRATION_INDEX :
- Attributes:
qualified_only- InOut:
Name
Initial
Comment
REFERENCE_WEIGHT_1
0
Value to set the current weight measured as “reference weight 1”
REFERENCE_WEIGHT_2
1
Value to set the current weight measured as “reference weight 2”
CALCULATION
2
Value to start the calucation with two points input reference weight and measurement record