ERROR_ID (ENUM)
TYPE ERROR_ID
- Attributes:
qualified_only- InOut:
Name
Initial
Comment
NO_ERROR
16#0
No error
ERR_VALUE_INVALID
16#1
At least one field of the value is not supported
ERR_VALUE_TOO_LOW
16#2
Value is less than “LowerLimit” of weight specified
ERR_VALUE_TOO_HIGH
16#3
Value is greater than “UpperLimit” of weight specified
ERR_PARAMETER_ERROR
16#4
Value of parameter is invalid or not supported by module
ERR_FUNCTION_CODE
16#5
Function code is not supported by module
ERR_FAILURE
16#6
Failure to obtain the measurement
ERR_OVERRUN
16#7
The previous value is overwritten by new measurement before fetching when ower sampling rate is faster than cycletime of task
ERR_OCCUPY_CHANNEL
16#8
The same strain gauge input channel has been called and executed by function block
ERR_EXCITATION
16#9
Excitation malfunction
ERROR_WRONG_ADDRESS
16#A
Invalid channel address, the address must not be 0
ERR_BROKEN_WIRE
16#80
Broken wire of external connection
ERROR_SHORT_CIRCUIT
16#81
Short circuit of external connection
ERR_CHANNEL_OVERFLOW
16#82
Overflow of input signal
ERROR_CHANNEL_UNDERFLOW
16#83
Underflow of input signal
ERR_LOW_VOLTAGE
16#84
Voltage is too low to operate
ERROR_PARAMETER_RANGE
16#85
Invalid parameter, value is out of the range specified
ERR_PARAMETER_CRC
16#86
Invalid parameter block due to CRC error detected
ERROR_HARDWARE_ADC
16#87
ADC hardware malfunction
ERR_HARDWARE_REFERENCE
16#88
Internal reference voltage malfunction
ERROR_HARDWARE_COMMUNICATION
16#89
Internal communication error