IExternalUserDatabaseProvider.CheckLoginWithGroupID (METH)
METHOD CheckLoginWithGroupID : VUM_ReturnValues
This method checks whether the user is in the database, the password is correct and the user belongs to the user group. If everything is correct the function returns VUM_ReturnValues.ERR_OK. see VUM_ReturnValues (ENUM) where possible error reasons are described.
- InOut:
Scope
Name
Type
Comment
Return
CheckLoginWithGroupIDInput
wstUserNameWSTRINGthe user name
wstPasswordWSTRINGthe password of the user
dwUserGroupIDDWORDthe user group id to which the user must belong to
Output
wstFullNameWSTRINGthe full name of the user