VisuUserMgmtProvider.SetExtUsersToDisplayArray (METH)
METHOD SetExtUsersToDisplayArray : INT
This Method allows the use of custom sized arrays for use with the VisuUserMgmtProvider. It allows creating User-Management-Dialogs that can display a custom amount of available users. The Method, for example, can be called in the “Absolute Movement” Property on an Element in order to set a custom sized array. The Method returns always 0.
- InOut:
Scope
Name
Type
Return
SetExtUsersToDisplayArrayINTInput
arrPOINTER TO VUM_UserInternal
arrSizeUDINT