Visu_FbDateTimeProvider (FB)

FUNCTION_BLOCK Visu_FbDateTimeProvider

This FB provide the Current Local and UTC Time

InOut:

Scope

Name

Type

Initial

Comment

Input

enDateTimeLibrary

VisuEnumDateTimeLibrary

VisuEnumDateTimeLibrary.UseSysTimeRTC

Choose between the Time Library (Utils or SysTimeRTC)

tzTimeZone

Util.TimeZone

Time zone as base for calculating local time. It is only needed when use the Times from the Utils Library. For further infos to the type see in the Utils Library.

Methods:

ConvertLocalToUtcTime

ConvertUtcToLocalTime

GetCurrentLocalTime

GetCurrentUtcTime

Structure: