VisuFbTickMarkDrawer2.prvProcessMinorTickMarks (METH)
METHOD prvProcessMinorTickMarks
This method draws the minor tick marks.
- InOut:
Scope
Name
Type
Comment
Input
diNumMinorTickMarksDINTThe number of minor tick marks to draw
eWhichTickMarkVisuEnumMinorTickmarkA VisuEnumMinorTickmark value describing the kind of minor tick marks to draw
diIndexMajorDINTThe 0-relative index if the major tick mark the minor tick mark belongs to. Only relevant if eWhichTickMark = VisuEnumMinorTickmark.NORMAL
itfTickMarkProviderITickMarkProviderThe ITickMarkProvider instance providing the parameters for drawing the minor tick marks
vecDeltaVisuStructVectorSame parameter like in IPlotAxisTickMarkTraverserClient.ProcessMinorTickMarks
vecTickDirVisuStructVectorSame parameter like in IPlotAxisTickMarkTraverserClient.ProcessMinorTickMarks