Visu_ElemTrace_Versions (GVL)
take care when doing changes here, might be accessed from generated code
- Attributes:
qualified_only- InOut:
Scope
Name
Type
Initial
Comment
Constant
_VISUELEMTRACE_VERSION_LARGEROREQUAL_3_4_0_0
INT0
The following identifier are only used by the code generation to determine, whether the version of this library is greater or equal a given version
_VISUELEMTRACE_VERSION_LARGEROREQUAL_3_5_7_0
INT0
_VISUELEMTRACE_VERSION_LARGEROREQUAL_3_5_11_0
INT0