VisuFbElemTextEditor.prvGetTextContainingArea (METH)
METHOD prvGetTextContainingArea : VisuStructPaintRectangle
This method returns the rectangle, that describes the area, where the text will be displayed. That is approximately the rectangle of the texteditor without the vertical and horizontal
- / scrollbars (if visible). In detail: the vertical range of this area will be computed by the
number of visible lines and the line height, because below the last line there might be some vertical space, that will be not used.
- InOut:
Scope
Name
Type
Comment
Return
prvGetTextContainingAreaVisuStructPaintRectangleOutput
iLowermostYPosINTReturns the lowermost y position within the texteditor, where text can be displayed