ICompactTextListInfo2.GetUsedLINTTextids (METH)
METHOD GetUsedLINTTextids : POINTER TO ARRAY [0..0] OF LINT
returns the used textids in the texlist stTextListName. with the number of ids (GetNumberOfEntriesOfTextlist), it is possible to iterate through the ids, as they are stored in an array of lint and the returnvalue is the first value in the array
- InOut:
Scope
Name
Type
Return
GetUsedLINTTextidsPOINTER TO ARRAY [0..0] OF LINT
Input
stTextListNameSTRING