SymbolicVarNodeAccessor.EventCallback (METH)

METHOD EventCallback : RTS_IEC_RESULT

The interface ICmpEventCallback must be registered for an event. If this event is posted, this callback method is called.

InOut:

Scope

Name

Type

Comment

Return

EventCallback

RTS_IEC_RESULT

Input

pEventParam

POINTER TO CmpEventMgr.EventParam

Pointer to the event parameters, see Struct EventParam