POUTypeClass (GVL)
The three lower order bits of the third nibble designate the POU type.
- InOut:
Scope
Name
Type
Initial
Comment
Constant
TYPE_POU_FUNCTION
INT16#100
POU type function
TYPE_POU_FUNCTION_BLOCK
INT16#200
POU type function block
TYPE_POU_PROGRAM
INT16#300
POU type program
TYPE_POU_STRUCTURE
INT16#400
POU type structure
TYPE_POU_UNION
INT16#500
POU type union
TYPE_POU_UABUILTIN
INT16#1000
POU UA builtin type