ILeafTreeNode (ITF)

INTERFACE ILeafTreeNode EXTENDS __SYSTEM.IQueryInterface

The ILeafTreeNode interface is not meant to be used by end users, it is considered internal to the symbol configuration and data server. If you want to access the symbol information, use the interfaces defined in the IIecVarAccess_Itfs instead.

Properties:

abstrNodeType

Methods:

ExecuteCall

ExecuteCall2

Get

GetAccessRights

GetAccessRights2

GetAddress

GetAddress3

GetAttributeByIndex

GetClientOffset

GetFlags

GetNamespaceNodeFlags

GetNumOfAttributes

GetSize

GetType

NodeFound

Set

Swap2

Structure: