IRecipeDefinition3.GetRecipeValuesSizeOf (METH)
METHOD GetRecipeValuesSizeOf : DWORD
Returns the recipe values from the corresponding recipe.
Possible last error values: ERR_NO_RECIPE_MANAGER_SET, ERR_RECIPE_DEFINITION_NOT_FOUND, ERR_RECIPE_NOT_FOUND, ERR_FAILED, ERR_OK
- InOut:
Scope
Name
Type
Comment
Return
GetRecipeValuesSizeOfDWORDInput
pStringsPOINTER TO ARRAY [0..0] OF STRING
The strings where the recipe values should be stored
iSizeINTSize of the string array.
iStartIndexINTStart index. Can be used for a scroll function (See example)
iSizeOfStringINTSize of one string in the pStrings array