ReturnValues (GVL)
- InOut:
Scope
Name
Type
Initial
Comment
Constant
ERR_OK
UDINT16#0
The operation succeeded
ERR_FAILED
UDINT16#1
The operation failed
ERR_PARAMETER
UDINT16#2
Wrong parameter
ERR_NOTINITIALIZED
UDINT16#3
The dataserver object is not initialized. The dataserver is necessary if the recipe management is used in combination with the CODESYS HMI.
ERR_NOTIMPLEMENTED
UDINT16#C
The dataserver does not implement the interface IDataServer4, which is necessary if the recipe management is used in combination with the CODESYS HMI.
ERR_NO_OBJECT
UDINT16#10
Not all recipe definition variables can be written via the dataserver. Only the valid recipe definition variables are written.
ERR_NOMEMORY
UDINT16#11
The dataserver did not get enough memory
ERR_RECIPE_FILE_NOT_FOUND
UDINT16#4000
The recipe file was not found.
ERR_RECIPE_MISMATCH
UDINT16#4001
The content of the recipe file does not match the current recipe. This error is only generated when the storage type is textual (see “RecipeManager” “Storage Type” in your project) and when a variable name in the file does not match the variable name in the recipe definition. The recipe file is not loaded when this error occurs.
Possible reasons:
A variable has been removed in the recipe definition of the project.
ERR_RECIPE_SAVE_ERR
UDINT16#4002
The save operation failed.Possible reasons:The file cannot be created or opened because the disk is full.
The configured file path does not exist (see “RecipeManager” “File Path” in your project).
The configured file extension is not allowed by the runtime (see “RecipeManager” “File Extension” in your project).
ERR_RECIPE_NOT_FOUND
UDINT16#4003
The recipe does not exist
ERR_RECIPE_DEFINITION_NOT_FOUND
UDINT16#4004
The recipe definition does not exist
ERR_RECIPE_ALREADY_EXIST
UDINT16#4005
The recipe already exists in the recipe definition. Use another name to create a new recipe.
ERR_NO_RECIPE_MANAGER_SET
UDINT16#4006
The global recipe manager is not set.Possible reasons:This can happen when the option recipe management in plc is not set in the recipe manager of the current application.
ERR_RECIPE_NOT_ALL_VARIABLES_WERE_LOADED
UDINT16#4007
The recipe definition contains more variables than the recipe file. In this case the variable values from the recipe file are written anyway. This is only an info not an error.
ERR_RECIPE_NOMEMORY
UDINT16#4008
The recipe definition has no free memory to create an new recipe.Possible reasons:This can happen when the option “save recipe changes to recipe files automatically” is not set in the recipe manager of the current application. In this case only 50 recipes per recipe definition are possible.
If the option “save recipe changes to recipe files automatically” is set the error cannot happen. When the disk is full the error ERR_RECIPE_SAVE_ERR is created.
ERR_RECIPE_MANAGER_LOCKED_DURING_ONLINE_CHANGE
UDINT16#4009
The recipe manager was locked during online change.Possible reasons:Some of the recipe man commands should be executed while an online change occurs. These commands were not executed during online change.
ERR_SOURCE_EXHAUSTED
UDINT16#40A0
Used for UTF8 helper
ERR_TARGET_EXHAUSTED
UDINT16#40A1
Used for UTF8 helper
ERR_SOURCE_ILLEGAL
UDINT16#40A2
Used for UTF8 helper