InfoValues (ENUM)
TYPE InfoValues :
- Attributes:
qualified_only- InOut:
Name
Initial
Comment
NO_INFO
16#0
INFO_RECIPE_MANAGER_NOT_ALL_VARIABLES_FOUND
16#1
During load recipe, with the load type “Load matching variables by variable name”, some variables from the application variable list were NOT in the recipe file.Possible reason: The application recipe definition was extended by new variables and the recipe file is older.INFO_RECIPE_MANAGER_OTHER_VARIABLES_FOUND
16#2
During load recipe, with the load type “Load matching variables by variable name”, some variables from the recipe file were not in the application variable list.Possible reason: Some variables where deleted in the application variable list and the recipe file is older.INFO_RECIPE_MANAGER_ONE_OR_MORE_VARIABLES_FOUND
16#4
During load recipe, with the load type “Load matching variables by variable name”, one ore more values were written into the application recipe.Possible reason: One or more variables were found in the recipe file which match to the application variable list.INFO_RECIPE_MANAGER_ALL_VARIABLES_FOUND
16#8
During load recipe, with the load type “Load matching variables by variable name”, all values were written into the application recipe.Possible reason: All variables were found in the recipe file which match to the application variable list.