IMData_Write (FB)
FUNCTION_BLOCK IMData_Write
Write I&M Data of specified submodule
- InOut:
Scope
Name
Type
Comment
Input
xExecuteBOOLRising edge: Start Operation DCP-Get
IDDWORDThe ID of the submodule
IM_Tag_FunctionSTRING(32)Function of the submodule
IM_Tag_LocationSTRING(22)Location of the submodule
IM_DateSTRING(16)Date-Format “YYYY-MM-DD’T’HH:MM’Z’” or “YYYY-MM- DD’T’HH:MM’±HH:MM’” (ISO 8601-1)
IM_DescriptorSTRING(54)Additional information on the submodule
Output
xDoneBOOLAction successfully completed
xBusyBOOLFunction block active
xErrorBOOLTRUE: error occurred, function block aborts actionSTATUSUDINTService failed, or at least one of the requested options is not valid