CTLPBE_State (ENUM)

TYPE CTLPBE_State :

Attributes:
qualified_only
InOut:

Name

Comment

IDLE

Wait for the start of DATA

START

Wait for a PrmBegin command

WFBCNF

Wait for a PrmBegin confirmation from the IO device

WFREQ

The application shall convey the records to the IO device using the CTLWRI.

WFECNF

Wait for a PrmEnd confirmation from the IO device

WFIND

Wait for an application ready indication from the IO device

WFRSP

Wait for an application ready confirmation from the application and convey it to the IO device.