PNSlave.CheckCurrentSupportedCommunicationState (METH)
METHOD CheckCurrentSupportedCommunicationState : BOOL
Returns true if the driver in the current state supports the requested communications state The method CheckSupportedCommunicationState is used to check for the general availability of communications states Therefore the result of CheckCurrentSupportedCommunicationState and CheckSupportedCommunicationState could differ if the driver is for example in the startup procedure and not supporting currently some communication states.
- InOut:
Scope
Name
Type
Comment
Return
CheckCurrentSupportedCommunicationStateBOOLInput
eRequestedStateDED.DEVICE_TRANSITION_STATEThe communication state to check