SAdapterFlags (STRUCT)
TYPE SAdapterFlags : STRUCT
- InOut:
Name
Type
Comment
INACTIVEBITInterface not ready for ip communication (no driver, no ip address, no link, …)
ALIAS_IPBITFurther ip (aka alias address) of adapter
DYNAMIC_IPBITDynamic ip address, provided by DHCP, BOOTP, etc. Cannot be changed by SysSockSetIpAddressAndNetMask()
FIX_IPBITFix (e. g. hard coded) ip address. Cannot be changed by SysSockSetIpAddressAndNetMask()
IP_CHANGE_ALLOWEDBITAdapter is white listed to allow address changes. If non of the flags SOCK_AIF_DYNAMIC_IP or SOCK_AIF_FIX_IP is set, the ip address can be likely changed by SysSockSetIpAddressAndNetMask()
GATEWAY_INFO_VALIDBITDefaultGateway address is valid. Is not set, if no Gateway information is provided by the system.
INFO_VALIDBITAdapter is valid - only valid adapters are returned by SysSockGetFirstAdapterInfo() or SysSockGetNextAdapterInfo()