IoDrvEthernetDiag.UpdateConfiguredInterfaceName (METH)
METHOD UpdateConfiguredInterfaceName : ErrorCode
This method updates the configured Ethernet interface of the ethernet node The device must be in disabled state (via Enable, see also DED.Reconfigure), else the update is rejected.
- InOut:
Scope
Name
Type
Comment
Return
UpdateConfiguredInterfaceNameInput
NICNameWSTRINGthe name of the network interface to be used