IoDrvEtherNetIP_diag (FB)

FUNCTION_BLOCK IoDrvEtherNetIP_diag EXTENDS IoDrvEtherNetIP IMPLEMENTS DED.IBus, DED.IStack, DED.IReconfigureProvider, IoDrvEtherNetIPAdapter.IReconfigureHandshake

Driver FB: Don´t create this FB directly.

InOut:

Scope

Name

Type

Initial

Comment

Inherited from

Input

xReset

BOOL

Rising edge to reset the scanner.

IoDrvEtherNetIP

Output

eState

ScannerState

ScannerState.UPDATE_CONFIGURATION

State of the EtherNet/IP Scanner see ScannerState

IoDrvEtherNetIP

eError

ERROR

Specifies the error, if scanner is in error state see ERROR

IoDrvEtherNetIP

Properties:

ChildNodeCount

Connector

Enable

FirstChildNode

IsRootNode

MaximumExplicitMessageSize, inherited from IoDrvEtherNetIP

NextSiblingNode

ParentNode

SiblingNodeCount

State, inherited from IoDrvEtherNetIP

Methods:

GetBusInfo

GetBusState

GetDeviceInfo

GetDeviceState

IOCycle, inherited from IoDrvEtherNetIP

ServiceCycle, inherited from IoDrvEtherNetIP

SetCommunicationState

Structure: