IoDrvCIFXProfinetDeviceDiag.GetSpecificDeviceErrorAsync (METH)

METHOD GetSpecificDeviceErrorAsync : DED.PROC_STATE

Returns the specific device error of the current node; interpretation is fieldbus-dependent; you can also use functionblock GetSpecificDeviceError

InOut:

Scope

Name

Type

Comment

Return

GetSpecificDeviceErrorAsync

DED.PROC_STATE

Input

eCmd

DED.PROC_CMD

eCommand

pData

CAA.PVOID

Pointer to memory

szSize

CAA.SIZE

Size of memory in bytes where pData is pointing to

Output

szCount

CAA.SIZE

Number of Bytes written to pData

eError

DED.ERROR

error code if method fails