IDatasourcesMgr2.CreatePersistantItemList (METH)
METHOD CreatePersistantItemList : IDataItemListPersistant
Creates an item list that will be registered automatically within the affected datasources after (re)connections of these datasources. An according list can be used in followup calls to IDatasourcesMgr.ReadItemsSync or IDatasourcesMgr.WriteItemsSync
Important
Having such lists might slow down the connection setup because the list has to be registered within the connected device!
Important
Using this method and the related ones working on the list requires according locking around using IDatasourcesMgr2.Lock and IDatasourcesMgr2.Unlock
Note
It is not supported to register several lists for the same usecase.
Note
Once the list is no longer necessary, it can be deleted using IDatasourcesMgr2.DeletePersistantItemList
- InOut:
Scope
Name
Type
Comment
Return
CreatePersistantItemListInput
usageThe usecase this list is intended for
usageDetailsWSTRINGSome details of the usage. In case of PersistantItemListUsage.Recipes this will be the name of the recipe definition.
udiInitialCapacityUDINTThe initial capacity of this list (will be extended if it becomes larger)
Output
resultSysTypes.RTS_IEC_RESULTAn error code providing additional information in case of creation problems