IDataItemList.CreateAndAdd (METH)
METHOD CreateAndAdd : SysTypes.RTS_IEC_RESULT
Creates a new item for monitoring and immediately adds it to the list.
Note
Usually items are monitored in total. If you want to expand the items (to prevent problems with different alignment etc.) then consider using the method IDataItemListExpanding.CreateAndAddExpanding instead.
- InOut:
Scope
Name
Type
Comment
Return
CreateAndAddSysTypes.RTS_IEC_RESULTAn error code representing the result of the operation. In case of success, ERR_OK will be returned
Input
pstSymbolPOINTER TO STRING
The symbolic name of the variable to activate. Here the name of the variable on the local PLC/HMI is expected.