IDriverStateMachine2.WaitingForCommSetting (METH)
METHOD WaitingForCommSetting : SysTypes.RTS_IEC_RESULT
- InOut:
Scope
Name
Type
Comment
Return
WaitingForCommSettingSysTypes.RTS_IEC_RESULTAn error code representing the result of this operation. In case an error happens, an according eror code should be returned. Please remark that this operation is not expected to return ERR_PENDING. A successfull return (ERR_OK) of this method will then cause followup calls to IDriverStateMachine.StartConnect.
Input
xPreviewBOOL