IDriverRequestFactoryLargeRequests.CreateLargeReadRequest (METH)
METHOD CreateLargeReadRequest : IDriverLargeRequest
Creates a request representing the read operation for the given list of items. The request may stay alive until the list of items changes. That means it might be issued in several calls to IDriverStateMachine.SendRequest When the request is no longer necessary, it will be released by a call to IDriverRequestFactory.ReleaseRequest In contrast to IDriverRequestFactory.CreateReadRequest, the resulting request might require being sent using several calls to IDriverStateMachine.SendRequest for completion.
Important
The items may be stored as part of the request object. Nevertheless it is not allowed to access them from other threads because the list might change within the main datasources task. The list will not change as long as this object is alive.
- InOut:
Scope
Name
Type
Comment
Return
CreateLargeReadRequestA new request object representing the read operation for the given list of items.
Input
pItemsPOINTER TO IDataItem
A pointer to an array of IDataItem instances that should be monitored.
itemsCountDINTThe number of items within the array.