CDSV3Request.SetContentData (METH)
METHOD SetContentData : IDatasources.SysTypes.RTS_IEC_RESULT
Assigns the content of the CODESYS V3 Service that should be sent
- InOut:
Scope
Name
Type
Comment
Return
SetContentDataIDatasources.SysTypes.RTS_IEC_RESULTAn error code representing the result of this operation.
Input
pDataPOINTER TO BYTE
A pointer to the data that should be sent by the service
Note
This data does not include the header part so only the service content must be used here.
Important
Please remark that this buffer must be valid until the response is received, ie. |ICustomRequestCallback.RequestFinished| is called for the current request
uxiSize__UXINTThe size of the data