OurVarInfo.ArrayAccessDetected (METH)
METHOD ArrayAccessDetected
If implemented, this method is called to notify about a valid array access that was parsed. By valid we understand that it is syntactically correct as well as within the allowed array range.*)
- InOut:
Scope
Name
Type
Comment
Input
pstrPOINTER TO STRING
The pointer to the beginning of the array access, ie. the opening parenthese ‘[’
lengthINTThe length of the array access within the string as it might not be 0 terminated after the closing parenthese. As an example, the value will be 3 for ‘[1]’ or 5 for ‘[3,4]’*)