RequestFactory.CreateReadRequest (METH)
METHOD CreateReadRequest : IDatasources.IDriverRequest
Creates a request representing the read operation for the given list of items. The request may stay alive until the list of items changes. That means it might be issued in several calls to |IDriverStateMachine.SendRequest| When the request is no longer necessary, it will be released by a call to |IDriverRequestFactory.ReleaseRequest|
Important
The items may be stored as part of the request object. Nevertheless it is not allowed to access them from other threads because the list might change within the main datasources task. The list will not change as long as this object is alive.
- InOut:
Scope
Name
Type
Comment
Return
CreateReadRequestIDatasources.IDriverRequestA new request object representing the read operation for the given list of items.
Input
pItemsPOINTER TO IDatasources.IDataItem
A pointer to an array of |IDataItem| instances that should be monitored.
itemsCountDINTThe number of items within the array.