IDataServer5.StartRecordMode (METH)
METHOD StartRecordMode : UDINT
Clients of the dataserver can call this method to start recording the following actions (UseData, ReleaseData). In between calls to this method and the according call to <see>GetRecordResult</see> no real action will be done. Instead the action will only be recorded. The result can be retrieved using <see>GetRecordResult</see>.
- InOut:
Scope
Name
Type
Return
StartRecordModeUDINT