DTCLogger (FB)

FUNCTION_BLOCK DTCLogger EXTENDS DTCHandlerBase

This function block can be connected to a DM1_Read or DM2_Read function block. As long as xEnable is TRUE it receives DTCs and writes it to the plc logger.

InOut:

Scope

Name

Type

Initial

Comment

Inherited from

Input

xEnable

BOOL

TRUE: Action starts
FALSE: Action stops, outputs xDone, xBusy, xError are resetted

LTrig

Output

xDone

BOOL

TRUE: Action successfully completed

LTrig

xBusy

BOOL

TRUE: Function block active

LTrig

xError

BOOL

TRUE: Error occurred, function block aborts action
FALSE: No error

LTrig

Input

itfDTCHandlerList

IDTCHandlerList

DMx_Read instance

DTCHandlerBase

Output

eError

ERROR

detailed error information if xError is TRUE

DTCHandlerBase

Input

hLogger

SysTypes.RTS_IEC_HANDLE

CmpLog.LOG_STD_LOGGER

Handle to the logger. Default: CmpLog.LOG_STD_LOGGER