MemMove (FUN)
FUNCTION MemMove : BOOL
The function copies the amount of “uiNumberOfBytes” of memory from memory area “Source” to “Destination”, wheras these memory areas are allowed to overlap! In case of success, the function will return “TRUE”. Only if “Source” or “Destination” are set to “0” the copying will not be carried out and the function will return “FALSE”.
- InOut:
Scope
Name
Type
Comment
Return
MemMoveBOOLfunction return “TRUE” if the moving of bytes succeeded
Input
pSourcePOINTER TO BYTE
address of source memory
pDestinationPOINTER TO BYTE
address of destination memory
uiNumberOfBytesUINTnumber of bytes to move