Encode (FUN)
FUNCTION Encode : BOOL
Function encodes “Source” (ARRAY OF DWORD) into “Destination” (ARRAY OF BYTE), meaning 1 DWORD is split up into 4 BYTEs. Assumes “uiNumberOfBytes” is a multiple of 4, whereas if it is not “FALSE” is returned.
- InOut:
Scope
Name
Type
Comment
Return
EncodeBOOLfunction returns “TRUE” if encoding succeeded
Input
pSourcePOINTER TO ARRAY [0..0] OF DWORD
address of source memory
pDestinationPOINTER TO ARRAY [0..0] OF BYTE
address of destination memory
uiNumberOfBytesUINTnumber of bytes to encode