Hysteresis_LREAL (FB)
FUNCTION_BLOCK Hysteresis_LREAL
This function block will set the output variable to
TRUE, if the input value \(x \in \mathbb{R}\) is smaller
than a lower bound \(x_{u} \in \mathbb{R}\).It will set the output variable to
FALSE, if the input value \(x\) exceeds the upper bound \(x_{o} \in \mathbb{R}\).If \(x\) lies between the lower and the upper bound, the value of the output variable will rest unchanged by the module.
- InOut:
Scope
Name
Type
Comment
Input
lrValueLREALinput value \(x \in \mathbb{R}\)
lrLimitPosLREALupper bound \(x_{o} \in \mathbb{R}\)
lrLimitNegLREALlower bound \(x_{u} \in \mathbb{R}\)
Output
xOutBOOLFALSE: If \(x > x_{o} \land x_{u} < x_{o}\)TRUE: If \(x < x_{u} \land x_{u} < x_{o}\)“xOut” else