Hysteresis_DINT (FB)
FUNCTION_BLOCK Hysteresis_DINT
This function block will set the output variable to
TRUE, if the integral value \(x \in \mathbb{Z}\)
is smaller than an integral lower bound \(x_{u} \in \mathbb{Z}\)It will set the Boolean output variable to
FALSE, if the input value \(x\) exceeds the integral upper bound \(x_{o} \in \mathbb{Z}\).If \(x\) lies between the lower and upper bound, the value of the output will rest unchanged by the module.
- InOut:
Scope
Name
Type
Comment
Input
diValueDINTinput value \(x \in \mathbb{Z}\)
diLimitPosDINTupper bound \(x_{o} \in \mathbb{Z}\)
diLimitNegDINTlower bound \(x_{u} \in \mathbb{Z}\)
Output
xOutBOOLFALSE: If \(x > x_{o} \land x_{u} < x_{o}\)TRUE: If \(x < x_{u} \land x_{u} < x_{o}\)“xOut” else