SetTimeZoneInformation (FB)

FUNCTION_BLOCK SetTimeZoneInformation

With this function block the specific information of the time zone can be modified. The time zone setting will be kept even after a Reset-Origin of the controller and can only be modified by being overwritten again. If no automatic switch is desired, all elements of tziInfo.stStandardDate and tziInfo.stDaylightDate must be set to 0.

InOut:

Scope

Name

Type

Comment

Input

xExecute

BOOL

Rising edge: Action start
Falling edge: Resets outputs. If a falling edge occurs before the function block has completed its action, the outputs operate in the usual manner and are only reset if either the action is completed or in the event of an error. In this case, the corresponding output values (xDone, xError, iError) are present at the outputs for exactly one cycle.

tziInfo

RTCLK_TIME_ZONE_INFO

Information on the time zone

Output

xDone

BOOL

Action successfully completed

xBusy

BOOL

Function block active

xError

BOOL

TRUE: error occurred, function block aborts action
FALSE: no error

eError

ERROR

Error description for diagnosis