SetDateAndTime (FB)
FUNCTION_BLOCK SetDateAndTime
This function block sets the realtime clock.
The current local time is passed in the parameter
dtDateAndTime.Note
If the time is within the not-unique interval shortly after the switch to standard (winter) time, standard time will be assumed. This case occurs for example in the Central European countries, if on the last Sunday of October the time is set at 2:30 a.m.. Here it is not clear, whether 2:30 a.m. is still summer time or already standard (winter) time. In this case the module assumes standard (winter) time.
- InOut:
Scope
Name
Type
Comment
Input
xExecuteBOOLRising edge: Action startFalling edge: Resets outputs. If a falling edge occurs before the function block has completed its action, the outputs operate in the usual manner and are only reset if either the action is completed or in the event of an error. In this case, the corresponding output values (xDone, xError, iError) are present at the outputs for exactly one cycle.dtDateAndTimeDTOutput
xDoneBOOLAction successfully completed
xBusyBOOLFunction block active
xErrorBOOLTRUE: error occurred, function block aborts actionFALSE: no erroreErrorError description for diagnosis