GetTimeZoneInformation (FB)
FUNCTION_BLOCK GetTimeZoneInformation
This function block reads the specific information on the time zone
(for further information see library CAA_RealTimeClock).
- InOut:
Scope
Name
Type
Comment
Input
xExecuteBOOLRising edge: Action startFalling edge: Resets outputs. If a falling edge occurs before the function block has completed its action, the outputs operate in the usual manner and are only reset if either the action is completed or in the event of an error. In this case, the corresponding output values (xDone, xError, iError) are present at the outputs for exactly one cycle.Output
xDoneBOOLAction successfully completed
xBusyBOOLFunction block active
xErrorBOOLTRUE: error occurred, function block aborts actionFALSE: no erroreErrorError description for diagnosis
tziInfoRTCLK.TIME_ZONE_INFOInformation on the time zone