CB_CALLBACK (STRUCT)
TYPE CB_CALLBACK : STRUCT
This data structure describes the callback conditions and -function.
- Attributes:
qualified_only- InOut:
Name
Type
Initial
Comment
pPOUFuncCAA.PVOIDCAA.gc_pNULL
Address of the function to be called
eEventEVENT.ALL_EVENTS
Trigger event or CB_ALL_EVENTS
eClassEVENT_CLASS.NO_CLASS
Event class (mask)
eSourceEVENT_SOURCE.NO_SOURCE
Event source