BACnetLifeSafetyPoint.GetFaultValues (METH)

METHOD GetFaultValues : CmpBACnet.IEC_BACNET_STATUS

Gets the Fault_Values of this BACnet object. The returned pointer is allocated with the corresponding data, whereas the user has to use FreeStackAllocatedMemory, to free the allocated memory after data usage.

InOut:

Scope

Name

Type

Comment

Return

GetFaultValues

CmpBACnet.IEC_BACNET_STATUS

Output

uiListCount

CmpBACnet.IEC_BACNET_ELEMENT_COUNT

The length of the list in the following pointer

pList

POINTER TO CmpBACnet.IEC_BACNET_LIFE_SAFETY_STATE

The returned Pointer gets filled with the data of the List AND (!) the data referenced within that list (i.e. strings, etc.). After usage, use FreeStackAllocatedMemory, to free the used memory.