BACnetLifeSafetyPoint (FB)
FUNCTION_BLOCK PUBLIC BACnetLifeSafetyPoint EXTENDS BACnetStaticObjectBase IMPLEMENTS IBACnetLifeSafetyPoint
FB reflecting a BACnet-LifeSafetyPoint-Object. All Properties of this FB give access to the client writeable BACnet-Properties of the reflected BACnet-Object, although the access is done not client sided (without checking access restrictions). Additionaly access is given for the Present_Value-Property, although the latter is not (always) client side writeable. Moreover access right behaviour which changes due to dynamically changing BACnet-Property-Sets is done by an Event-Callback (BACnetEventCallback), which is attached to the BACNET_CALLBACK_WRITE-Callback. Additionally see documentation of BACnetObjectBase.
Properties:
AckedTransitions
Description
DeviceType
DirectReading
EventAlgorithmInhibit
EventAlgorithmInhibitRef
EventDetectionEnable
EventEnable
EventMessageTexts
EventMessageTextsConfig
EventState
EventTimeStamps
MaintenanceRequired
Mode
NotificationClass
NotifyType
OperationExpected
OutOfService
PresentValue
ProfileName
Reliability
ReliabilityEvaluationInhibit
Setting
Silenced
StatusFlags
TimeDelay
TimeDelayNormal
TrackingValue
Units
NumberOfProperties, inherited from BACnetObjectBase
ObjectID, inherited from BACnetObjectBase
Methods:
GetAcceptedModes
GetAlarmValues
GetFaultValues
GetLifeSafetyAlarmValues
GetMemberOf
SetAcceptedModes
SetAlarmValues
SetFaultValues
SetLifeSafetyAlarmValues
SetMemberOf
GetBACnetAccumulatorRecordProperty, inherited from BACnetObjectBase
GetBACnetArraySizeOfProperty, inherited from BACnetObjectBase
GetBACnetArraySizeOfTwoProperties, inherited from BACnetObjectBase
GetBACnetBitStringProperty, inherited from BACnetObjectBase
GetBACnetBooleanProperty, inherited from BACnetObjectBase
GetBACnetClientCOVProperty, inherited from BACnetObjectBase
GetBACnetDateProperty, inherited from BACnetObjectBase
GetBACnetDateRangeProperty, inherited from BACnetObjectBase
GetBACnetDateTimeProperty, inherited from BACnetObjectBase
GetBACnetDevObjPropReferenceProperty, inherited from BACnetObjectBase
GetBACnetDoubleProperty, inherited from BACnetObjectBase
GetBACnetEnumeratedProperty, inherited from BACnetObjectBase
GetBACnetObjPropReferenceProperty, inherited from BACnetObjectBase
GetBACnetObjectIDProperty, inherited from BACnetObjectBase
GetBACnetPrescaleProperty, inherited from BACnetObjectBase
GetBACnetRealProperty, inherited from BACnetObjectBase
GetBACnetScaleProperty, inherited from BACnetObjectBase
GetBACnetSetpointReferenceProperty, inherited from BACnetObjectBase
GetBACnetSignedProperty, inherited from BACnetObjectBase
GetBACnetStringProperty, inherited from BACnetObjectBase
GetBACnetTimeProperty, inherited from BACnetObjectBase
GetBACnetTimeStampProperty, inherited from BACnetObjectBase
GetBACnetUnsignedProperty, inherited from BACnetObjectBase
GetPropertyAccessRight, inherited from BACnetObjectBase
GetPropertyCallbackAttachment, inherited from BACnetObjectBase
GetPropertyId, inherited from BACnetObjectBase
GetPropertyInstanceStackAllocContentBuffer, inherited from BACnetObjectBase
GetPropertyInstanceWithContentBuffer, inherited from BACnetObjectBase
IsBACnetDateTimePropertyUnspecified, inherited from BACnetObjectBase
IsPropertyExistent, inherited from BACnetObjectBase
IsPropertyWriteable, inherited from BACnetObjectBase
SetBACnetAccumulatorRecordProperty, inherited from BACnetObjectBase
SetBACnetBitStringProperty, inherited from BACnetObjectBase
SetBACnetBooleanProperty, inherited from BACnetObjectBase
SetBACnetClientCOVProperty, inherited from BACnetObjectBase
SetBACnetDateProperty, inherited from BACnetObjectBase
SetBACnetDateRangeProperty, inherited from BACnetObjectBase
SetBACnetDateTimeProperty, inherited from BACnetObjectBase
SetBACnetDateTimePropertyToUnspecified, inherited from BACnetObjectBase
SetBACnetDevObjPropReferenceProperty, inherited from BACnetObjectBase
SetBACnetDoubleProperty, inherited from BACnetObjectBase
SetBACnetEnumeratedProperty, inherited from BACnetObjectBase
SetBACnetObjPropReferenceProperty, inherited from BACnetObjectBase
SetBACnetObjectIDProperty, inherited from BACnetObjectBase
SetBACnetPrescaleProperty, inherited from BACnetObjectBase
SetBACnetRealProperty, inherited from BACnetObjectBase
SetBACnetScaleProperty, inherited from BACnetObjectBase
SetBACnetSetpointReferenceProperty, inherited from BACnetObjectBase
SetBACnetSignedProperty, inherited from BACnetObjectBase
SetBACnetStringProperty, inherited from BACnetObjectBase
SetBACnetTimeProperty, inherited from BACnetObjectBase
SetBACnetTimeStampProperty, inherited from BACnetObjectBase
SetBACnetUnsignedProperty, inherited from BACnetObjectBase
SetObjectName, inherited from BACnetObjectBase
SetPropertyAccessRight, inherited from BACnetObjectBase
SetPropertyCallbackAttachment, inherited from BACnetObjectBase
SetPropertyInstance, inherited from BACnetObjectBase
WritePropertyInstance, inherited from BACnetObjectBase
Structure:
BACnetLifeSafetyPoint.AckedTransitions(PROP)BACnetLifeSafetyPoint.Description(PROP)BACnetLifeSafetyPoint.DeviceType(PROP)BACnetLifeSafetyPoint.DirectReading(PROP)BACnetLifeSafetyPoint.EventAlgorithmInhibit(PROP)BACnetLifeSafetyPoint.EventAlgorithmInhibitRef(PROP)BACnetLifeSafetyPoint.EventDetectionEnable(PROP)BACnetLifeSafetyPoint.EventEnable(PROP)BACnetLifeSafetyPoint.EventMessageTexts(PROP)BACnetLifeSafetyPoint.EventMessageTextsConfig(PROP)BACnetLifeSafetyPoint.EventState(PROP)BACnetLifeSafetyPoint.EventTimeStamps(PROP)BACnetLifeSafetyPoint.GetAcceptedModes(METH)BACnetLifeSafetyPoint.GetAlarmValues(METH)BACnetLifeSafetyPoint.GetFaultValues(METH)BACnetLifeSafetyPoint.GetLifeSafetyAlarmValues(METH)BACnetLifeSafetyPoint.GetMemberOf(METH)BACnetLifeSafetyPoint.MaintenanceRequired(PROP)BACnetLifeSafetyPoint.Mode(PROP)BACnetLifeSafetyPoint.NotificationClass(PROP)BACnetLifeSafetyPoint.NotifyType(PROP)BACnetLifeSafetyPoint.OperationExpected(PROP)BACnetLifeSafetyPoint.OutOfService(PROP)BACnetLifeSafetyPoint.PresentValue(PROP)BACnetLifeSafetyPoint.ProfileName(PROP)BACnetLifeSafetyPoint.Reliability(PROP)BACnetLifeSafetyPoint.ReliabilityEvaluationInhibit(PROP)BACnetLifeSafetyPoint.SetAcceptedModes(METH)BACnetLifeSafetyPoint.SetAlarmValues(METH)BACnetLifeSafetyPoint.SetFaultValues(METH)BACnetLifeSafetyPoint.SetLifeSafetyAlarmValues(METH)BACnetLifeSafetyPoint.SetMemberOf(METH)BACnetLifeSafetyPoint.Setting(PROP)BACnetLifeSafetyPoint.Silenced(PROP)BACnetLifeSafetyPoint.StatusFlags(PROP)BACnetLifeSafetyPoint.TimeDelay(PROP)BACnetLifeSafetyPoint.TimeDelayNormal(PROP)BACnetLifeSafetyPoint.TrackingValue(PROP)BACnetLifeSafetyPoint.Units(PROP)